Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static BoundaryMemberSetPlanarMill.FeedUnitTypes |
BoundaryMemberSetPlanarMill.FeedUnitTypes.NONE
no feed rate unit
|
static BoundaryMemberSetPlanarMill.FeedUnitTypes |
BoundaryMemberSetPlanarMill.FeedUnitTypes.PER_MINUTE
use per minute as the feed rate unit
|
static BoundaryMemberSetPlanarMill.FeedUnitTypes |
BoundaryMemberSetPlanarMill.FeedUnitTypes.PER_REVOLUTION
use per revolution as the feed rate unit
|
Modifier and Type | Method and Description |
---|---|
BoundaryMemberSetPlanarMill.FeedUnitTypes |
BoundaryMemberSetPlanarMill.feedUnit()
Returns the feed rate unit
License requirements: None. |
static BoundaryMemberSetPlanarMill.FeedUnitTypes |
BoundaryMemberSetPlanarMill.FeedUnitTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BoundaryMemberSetPlanarMill.FeedUnitTypes |
BoundaryMemberSetPlanarMill.FeedUnitTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BoundaryMemberSetPlanarMill.FeedUnitTypes[] |
BoundaryMemberSetPlanarMill.FeedUnitTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BoundaryMemberSetPlanarMill.setFeedUnit(BoundaryMemberSetPlanarMill.FeedUnitTypes newUnit)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.