Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static BladeEdge.EdgePointType |
BladeEdge.EdgePointType.ALONG_BLADE_DIRECTION
along blade direction
|
static BladeEdge.EdgePointType |
BladeEdge.EdgePointType.ALONG_PART_AXIS
along part axis
|
static BladeEdge.EdgePointType |
BladeEdge.EdgePointType.NO_CURLING
no curling
|
Modifier and Type | Method and Description |
---|---|
BladeEdge.EdgePointType |
BladeEdge.bladeEdgePoint()
Returns the Blade Edge Point
License requirements: None. |
static BladeEdge.EdgePointType |
BladeEdge.EdgePointType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BladeEdge.EdgePointType |
BladeEdge.EdgePointType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BladeEdge.EdgePointType[] |
BladeEdge.EdgePointType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BladeEdge.setBladeEdgePoint(BladeEdge.EdgePointType bladeEdgePoint)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.