public static class TurnToolBuilder.ReliefAngleTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_A3
Relief angle type: A (3)
|
static int |
_B5
Relief angle type: B (5)
|
static int |
_C7
Relief angle type: C (7)
|
static int |
_D15
Relief angle type: D (15)
|
static int |
_E20
Relief angle type: E (20)
|
static int |
_F25
Relief angle type: F (25)
|
static int |
_G30
Relief angle type: G (30)
|
static int |
_N0
Relief angle type: N (0)
|
static int |
_OOTHER
Relief angle type: O (other)
|
static int |
_P11
Relief angle type: P (11)
|
static TurnToolBuilder.ReliefAngleTypes |
A3
Relief angle type: A (3)
|
static TurnToolBuilder.ReliefAngleTypes |
B5
Relief angle type: B (5)
|
static TurnToolBuilder.ReliefAngleTypes |
C7
Relief angle type: C (7)
|
static TurnToolBuilder.ReliefAngleTypes |
D15
Relief angle type: D (15)
|
static TurnToolBuilder.ReliefAngleTypes |
E20
Relief angle type: E (20)
|
static TurnToolBuilder.ReliefAngleTypes |
F25
Relief angle type: F (25)
|
static TurnToolBuilder.ReliefAngleTypes |
G30
Relief angle type: G (30)
|
static TurnToolBuilder.ReliefAngleTypes |
N0
Relief angle type: N (0)
|
static TurnToolBuilder.ReliefAngleTypes |
OOTHER
Relief angle type: O (other)
|
static TurnToolBuilder.ReliefAngleTypes |
P11
Relief angle type: P (11)
|
Modifier and Type | Method and Description |
---|---|
static TurnToolBuilder.ReliefAngleTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnToolBuilder.ReliefAngleTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnToolBuilder.ReliefAngleTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final TurnToolBuilder.ReliefAngleTypes A3
public static final TurnToolBuilder.ReliefAngleTypes B5
public static final TurnToolBuilder.ReliefAngleTypes C7
public static final TurnToolBuilder.ReliefAngleTypes D15
public static final TurnToolBuilder.ReliefAngleTypes E20
public static final TurnToolBuilder.ReliefAngleTypes F25
public static final TurnToolBuilder.ReliefAngleTypes G30
public static final TurnToolBuilder.ReliefAngleTypes N0
public static final TurnToolBuilder.ReliefAngleTypes P11
public static final TurnToolBuilder.ReliefAngleTypes OOTHER
public static final int _A3
public static final int _B5
public static final int _C7
public static final int _D15
public static final int _E20
public static final int _F25
public static final int _G30
public static final int _N0
public static final int _P11
public static final int _OOTHER
public static TurnToolBuilder.ReliefAngleTypes valueOf(int value)
public static TurnToolBuilder.ReliefAngleTypes valueOf(String name)
public static TurnToolBuilder.ReliefAngleTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.