public static class TurnAvoidanceApproachBuilder.ApproachPathModes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
Path is inactive.
|
static int |
_POINTS
Path is defined by points.
|
static int |
_POINTS_AFTER_TOOL_CHANGE
Path is defined by points, but applied only after tool change.
|
static TurnAvoidanceApproachBuilder.ApproachPathModes |
NONE
Path is inactive.
|
static TurnAvoidanceApproachBuilder.ApproachPathModes |
POINTS
Path is defined by points.
|
static TurnAvoidanceApproachBuilder.ApproachPathModes |
POINTS_AFTER_TOOL_CHANGE
Path is defined by points, but applied only after tool change.
|
Modifier and Type | Method and Description |
---|---|
static TurnAvoidanceApproachBuilder.ApproachPathModes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceApproachBuilder.ApproachPathModes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceApproachBuilder.ApproachPathModes[] |
values()
Returns an array that contains the values for this enum.
|
public static final TurnAvoidanceApproachBuilder.ApproachPathModes NONE
public static final TurnAvoidanceApproachBuilder.ApproachPathModes POINTS
public static final TurnAvoidanceApproachBuilder.ApproachPathModes POINTS_AFTER_TOOL_CHANGE
public static final int _NONE
public static final int _POINTS
public static final int _POINTS_AFTER_TOOL_CHANGE
public static TurnAvoidanceApproachBuilder.ApproachPathModes valueOf(int value)
public static TurnAvoidanceApproachBuilder.ApproachPathModes valueOf(String name)
public static TurnAvoidanceApproachBuilder.ApproachPathModes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.