public static class PitchSetting.OutputUnitTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LEAD
Lead
|
static int |
_PITCH
Pitch
|
static int |
_SAME_AS_INPUT
Same as Input
|
static int |
_THREADS_PER_UNIT
Threads per mm
|
static PitchSetting.OutputUnitTypes |
LEAD
Lead
|
static PitchSetting.OutputUnitTypes |
PITCH
Pitch
|
static PitchSetting.OutputUnitTypes |
SAME_AS_INPUT
Same as Input
|
static PitchSetting.OutputUnitTypes |
THREADS_PER_UNIT
Threads per mm
|
Modifier and Type | Method and Description |
---|---|
static PitchSetting.OutputUnitTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PitchSetting.OutputUnitTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PitchSetting.OutputUnitTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final PitchSetting.OutputUnitTypes SAME_AS_INPUT
public static final PitchSetting.OutputUnitTypes PITCH
public static final PitchSetting.OutputUnitTypes LEAD
public static final PitchSetting.OutputUnitTypes THREADS_PER_UNIT
public static final int _SAME_AS_INPUT
public static final int _PITCH
public static final int _LEAD
public static final int _THREADS_PER_UNIT
public static PitchSetting.OutputUnitTypes valueOf(int value)
public static PitchSetting.OutputUnitTypes valueOf(String name)
public static PitchSetting.OutputUnitTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.