public static class InspectionGraphicalReportBuilder.GraphicalReportFilterType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_POINTS
Point based
|
static int |
_TOLERANCES
Tolerance based
|
static InspectionGraphicalReportBuilder.GraphicalReportFilterType |
POINTS
Point based
|
static InspectionGraphicalReportBuilder.GraphicalReportFilterType |
TOLERANCES
Tolerance based
|
Modifier and Type | Method and Description |
---|---|
static InspectionGraphicalReportBuilder.GraphicalReportFilterType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionGraphicalReportBuilder.GraphicalReportFilterType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionGraphicalReportBuilder.GraphicalReportFilterType[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionGraphicalReportBuilder.GraphicalReportFilterType TOLERANCES
public static final InspectionGraphicalReportBuilder.GraphicalReportFilterType POINTS
public static final int _TOLERANCES
public static final int _POINTS
public static InspectionGraphicalReportBuilder.GraphicalReportFilterType valueOf(int value)
public static InspectionGraphicalReportBuilder.GraphicalReportFilterType valueOf(String name)
public static InspectionGraphicalReportBuilder.GraphicalReportFilterType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.