public static class CAMSetup.OutputUnits extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INCH
use inch as output unit
|
static int |
_METRIC
use metric as output unit
|
static int |
_POST_DEFINED
use post defined unit as output unit
|
static CAMSetup.OutputUnits |
INCH
use inch as output unit
|
static CAMSetup.OutputUnits |
METRIC
use metric as output unit
|
static CAMSetup.OutputUnits |
POST_DEFINED
use post defined unit as output unit
|
Modifier and Type | Method and Description |
---|---|
static CAMSetup.OutputUnits |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAMSetup.OutputUnits |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAMSetup.OutputUnits[] |
values()
Returns an array that contains the values for this enum.
|
public static final CAMSetup.OutputUnits INCH
public static final CAMSetup.OutputUnits METRIC
public static final CAMSetup.OutputUnits POST_DEFINED
public static final int _INCH
public static final int _METRIC
public static final int _POST_DEFINED
public static CAMSetup.OutputUnits valueOf(int value)
public static CAMSetup.OutputUnits valueOf(String name)
public static CAMSetup.OutputUnits[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.