Package | Description |
---|---|
nxopen.cae.xyplot |
Provides classes and interfaces for XY Graphing.
|
Modifier and Type | Field and Description |
---|---|
static LimitsType |
LimitsType.FIXED_LIMITS
Type to use customized data limits as axis limits
|
static LimitsType |
LimitsType.FREE_LIMITS
Type to use source data limits as axis limits
|
static LimitsType |
LimitsType.OPTIMIZED_LIMITS
Type to optimize source data limits to natural axis limits
|
Modifier and Type | Method and Description |
---|---|
LimitsType |
AxisStyleSetting.limitsType()
Returns the limits type
License requirements: None. |
static LimitsType |
LimitsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LimitsType |
LimitsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LimitsType[] |
LimitsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AxisStyleSetting.setLimitsType(LimitsType limitsType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.