public class LimitsType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FIXED_LIMITS
Type to use customized data limits as axis limits
|
static int |
_FREE_LIMITS
Type to use source data limits as axis limits
|
static int |
_OPTIMIZED_LIMITS
Type to optimize source data limits to natural axis limits
|
static LimitsType |
FIXED_LIMITS
Type to use customized data limits as axis limits
|
static LimitsType |
FREE_LIMITS
Type to use source data limits as axis limits
|
static LimitsType |
OPTIMIZED_LIMITS
Type to optimize source data limits to natural axis limits
|
Modifier and Type | Method and Description |
---|---|
static LimitsType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LimitsType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LimitsType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LimitsType FREE_LIMITS
public static final LimitsType OPTIMIZED_LIMITS
public static final LimitsType FIXED_LIMITS
public static final int _FREE_LIMITS
public static final int _OPTIMIZED_LIMITS
public static final int _FIXED_LIMITS
public static LimitsType valueOf(int value)
public static LimitsType valueOf(String name)
public static LimitsType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.