Package | Description |
---|---|
nxopen.cae.xyplot |
Provides classes and interfaces for XY Graphing.
|
Modifier and Type | Field and Description |
---|---|
static AnchorType |
AnchorType.ABS_PERCENTAGE
the position of the point in the set abscissa percentage
|
static AnchorType |
AnchorType.END
the position of end point in a record display
|
static AnchorType |
AnchorType.MAXIMUM_VALUE
the position of the point which has maximum value in a record display
|
static AnchorType |
AnchorType.MINIMUM_VALUE
the position of the point which has minimum value in a record display
|
static AnchorType |
AnchorType.NONE
the normal marker without anchor type
|
static AnchorType |
AnchorType.START
the position of start point in a record display
|
Modifier and Type | Method and Description |
---|---|
AnchorType |
MarkerStyleSetting.attachmentType()
Returns the attachment type for associative marker
License requirements: None. |
static AnchorType |
AnchorType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AnchorType |
AnchorType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AnchorType[] |
AnchorType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
MarkerModel |
Graph.createAssociativeMarker(int recordIndex,
AnchorType attachType,
double absPercentage)
Creates an associative marker.
|
Graph.AnchorPointOfRecordData |
Graph.getAnchorPointOfRecord(int recordIndex,
AnchorType anchorType)
Gets anchor point of a record.
|
void |
MarkerStyleSetting.setAttachmentType(AnchorType anchorType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.