public class AnchorType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ABS_PERCENTAGE
the position of the point in the set abscissa percentage
|
static int |
_END
the position of end point in a record display
|
static int |
_MAXIMUM_VALUE
the position of the point which has maximum value in a record display
|
static int |
_MINIMUM_VALUE
the position of the point which has minimum value in a record display
|
static int |
_NONE
the normal marker without anchor type
|
static int |
_START
the position of start point in a record display
|
static AnchorType |
ABS_PERCENTAGE
the position of the point in the set abscissa percentage
|
static AnchorType |
END
the position of end point in a record display
|
static AnchorType |
MAXIMUM_VALUE
the position of the point which has maximum value in a record display
|
static AnchorType |
MINIMUM_VALUE
the position of the point which has minimum value in a record display
|
static AnchorType |
NONE
the normal marker without anchor type
|
static AnchorType |
START
the position of start point in a record display
|
Modifier and Type | Method and Description |
---|---|
static AnchorType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AnchorType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AnchorType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AnchorType NONE
public static final AnchorType START
public static final AnchorType END
public static final AnchorType MAXIMUM_VALUE
public static final AnchorType MINIMUM_VALUE
public static final AnchorType ABS_PERCENTAGE
public static final int _NONE
public static final int _START
public static final int _END
public static final int _MAXIMUM_VALUE
public static final int _MINIMUM_VALUE
public static final int _ABS_PERCENTAGE
public static AnchorType valueOf(int value)
public static AnchorType valueOf(String name)
public static AnchorType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.