Package | Description |
---|---|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Field and Description |
---|---|
static StrengthStressCriteria |
StrengthStressCriteria.MAX_PRINCIPLE |
static StrengthStressCriteria |
StrengthStressCriteria.MIN_PRINCIPLE |
static StrengthStressCriteria |
StrengthStressCriteria.VON_MISES |
Modifier and Type | Method and Description |
---|---|
StrengthStressCriteria |
StrengthResultsEvaluationSettingBuilder.stressCriteriaType()
Returns the stress criteria type
License requirements: nx_response_anlys ("NX Response Analysis") . |
static StrengthStressCriteria |
StrengthStressCriteria.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StrengthStressCriteria |
StrengthStressCriteria.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StrengthStressCriteria[] |
StrengthStressCriteria.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StrengthResultsEvaluationSettingBuilder.setStressCriteriaType(StrengthStressCriteria stressCriteria)
License requirements: nx_response_anlys ("NX Response Analysis") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.