Package | Description |
---|---|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Field and Description |
---|---|
static NodalFunctionEvalBeamLocation |
NodalFunctionEvalBeamLocation.ALL
All four Stress Recovery points on a beam cross section
|
static NodalFunctionEvalBeamLocation |
NodalFunctionEvalBeamLocation.C
Stress Recovery point C on a beam cross section
|
static NodalFunctionEvalBeamLocation |
NodalFunctionEvalBeamLocation.D
Stress Recovery point D on a beam cross section
|
static NodalFunctionEvalBeamLocation |
NodalFunctionEvalBeamLocation.E
Stress Recovery point E on a beam cross section
|
static NodalFunctionEvalBeamLocation |
NodalFunctionEvalBeamLocation.F
Stress Recovery point F on a beam cross section
|
Modifier and Type | Method and Description |
---|---|
NodalFunctionEvalBeamLocation |
NodalFunctionEvaluationSettingBuilder.beamDataLocation()
Returns the evaluation location of beam element, which is available when
EvaluationResultType is
EvaluationResultType.STRESS , or
EvaluationResultType.STRAIN
License requirements: nx_response_anlys ("NX Response Analysis") Created in NX9.0.0 |
static NodalFunctionEvalBeamLocation |
NodalFunctionEvalBeamLocation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NodalFunctionEvalBeamLocation |
NodalFunctionEvalBeamLocation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NodalFunctionEvalBeamLocation[] |
NodalFunctionEvalBeamLocation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NodalFunctionEvaluationSettingBuilder.setBeamDataLocation(NodalFunctionEvalBeamLocation beamLocation)
License requirements: nx_response_anlys ("NX Response Analysis") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.