Package | Description |
---|---|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ExcitationBuilder.ExcitationLocationType |
ExcitationBuilder.ExcitationLocationType.DISTRIBUTED_LOAD |
static ExcitationBuilder.ExcitationLocationType |
ExcitationBuilder.ExcitationLocationType.ENFORCED_MOTION |
static ExcitationBuilder.ExcitationLocationType |
ExcitationBuilder.ExcitationLocationType.NODAL_FORCE |
static ExcitationBuilder.ExcitationLocationType |
ExcitationBuilder.ExcitationLocationType.STATIC_LOAD |
Modifier and Type | Method and Description |
---|---|
ExcitationBuilder.ExcitationLocationType |
ExcitationLocationDefinition.excitationLocationType()
Returns the type of excitaion location
License requirements: nx_response_anlys ("NX Response Analysis") . |
static ExcitationBuilder.ExcitationLocationType |
ExcitationBuilder.ExcitationLocationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExcitationBuilder.ExcitationLocationType |
ExcitationBuilder.ExcitationLocationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExcitationBuilder.ExcitationLocationType[] |
ExcitationBuilder.ExcitationLocationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExcitationLocationDefinition.setExcitationLocationType(ExcitationBuilder.ExcitationLocationType excitationLocationType)
License requirements: nx_response_anlys ("NX Response Analysis") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.