Package | Description |
---|---|
nxopen.cae.qualityaudit |
Provides classes and interfaces relating to Quality Audit.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ComponentSynthesis
This action has as result a list of components and the connections using them.
|
interface |
ConnectionDistanceCheck
This action checks the distance between connections.
|
interface |
ConnectionPointsDistanceCheck
This action checks the distance between connection's definition points.
|
interface |
ConnectivityCheck
This action's output is a list of connected groups together with the involved connections.
|
interface |
DiameterCheck
This action performs checks on connections supporting diameter and displays errors when diameter is different from the expected one.
|
interface |
FreeEdgeDistanceCheck
This action checks if there are connections that are too close to the edge based on a configurable tolerance.
|
interface |
ListConnections
This action has as result the list of all connections from the specified model.
|
interface |
ListNonModeledConnections
This action's output is a list of connections that are not realized.
|
interface |
MeshLevelProjectionCheck
This action has as output the list of failed projections of the universal connections at mesh level.
|
interface |
ObjectLevelProjectionCheck
This action has as output the list of failed projections of the universal connections at object level.
|
interface |
SupportSequenceCheck
This action's output is the list of connections having more than 2 supports with wrong order (e.g. first support between the second and third).
|
Modifier and Type | Method and Description |
---|---|
Action |
ActionSettings.action()
Returns the action using these settings
License requirements: None. |
Action |
ActionList.getAction(Action.Id id)
Get the action by id.
|
Action[] |
ActionList.getSelectedActions()
Returns an array of all selected actions.
|
Action |
Result.owningAction()
Returns the owning action that provides this result
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ActionList.deselect(Action pAction)
Deselect the specified action to avoid using it in the quality audit.
|
boolean |
ActionList.isSelected(Action pAction)
Tells if the action is to be used in the quality audit.
|
void |
Manager.performActions(Action[] inputActions,
NXObject[] pObjects)
This method performs checks on the selected objects.
|
void |
ActionList.select(Action pAction)
Select the specified action to be used in the quality audit.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.