Package | Description |
---|---|
nxopen.cae.modelcheck |
Provides classes and interfaces relating to Model Check.
|
Modifier and Type | Field and Description |
---|---|
static TestValueTypes.Validator |
TestValueTypes.Validator.GREAT_THAN
the check passes if the check result is great than the criteria value
|
static TestValueTypes.Validator |
TestValueTypes.Validator.GREAT_THAN_OR_EQUAL
the check passes if the check result is equal or great than the criteria value
|
static TestValueTypes.Validator |
TestValueTypes.Validator.NONE
indicates no criteria value defined, not necessary to compare the check result with criteria value
|
static TestValueTypes.Validator |
TestValueTypes.Validator.SMALL_THAN
the check passes if the check result is small than the criteria value
|
static TestValueTypes.Validator |
TestValueTypes.Validator.SMALL_THAN_OR_EQUAL
the check passes if the check result is equal or small than the criteria value
|
Modifier and Type | Method and Description |
---|---|
TestValueTypes.Validator |
ITestValue.getValidator()
Returns the validator type
License requirements: None. |
static TestValueTypes.Validator |
TestValueTypes.Validator.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TestValueTypes.Validator |
TestValueTypes.Validator.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TestValueTypes.Validator[] |
TestValueTypes.Validator.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.