public static class TestValueTypes.Validator extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_GREAT_THAN
the check passes if the check result is great than the criteria value
|
static int |
_GREAT_THAN_OR_EQUAL
the check passes if the check result is equal or great than the criteria value
|
static int |
_NONE
indicates no criteria value defined, not necessary to compare the check result with criteria value
|
static int |
_SMALL_THAN
the check passes if the check result is small than the criteria value
|
static int |
_SMALL_THAN_OR_EQUAL
the check passes if the check result is equal or small than the criteria value
|
static TestValueTypes.Validator |
GREAT_THAN
the check passes if the check result is great than the criteria value
|
static TestValueTypes.Validator |
GREAT_THAN_OR_EQUAL
the check passes if the check result is equal or great than the criteria value
|
static TestValueTypes.Validator |
NONE
indicates no criteria value defined, not necessary to compare the check result with criteria value
|
static TestValueTypes.Validator |
SMALL_THAN
the check passes if the check result is small than the criteria value
|
static TestValueTypes.Validator |
SMALL_THAN_OR_EQUAL
the check passes if the check result is equal or small than the criteria value
|
Modifier and Type | Method and Description |
---|---|
static TestValueTypes.Validator |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TestValueTypes.Validator |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TestValueTypes.Validator[] |
values()
Returns an array that contains the values for this enum.
|
public static final TestValueTypes.Validator NONE
public static final TestValueTypes.Validator GREAT_THAN
public static final TestValueTypes.Validator GREAT_THAN_OR_EQUAL
public static final TestValueTypes.Validator SMALL_THAN
public static final TestValueTypes.Validator SMALL_THAN_OR_EQUAL
public static final int _NONE
public static final int _GREAT_THAN
public static final int _GREAT_THAN_OR_EQUAL
public static final int _SMALL_THAN
public static final int _SMALL_THAN_OR_EQUAL
public static TestValueTypes.Validator valueOf(int value)
public static TestValueTypes.Validator valueOf(String name)
public static TestValueTypes.Validator[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.