Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static XyFunctionMacroType |
XyFunctionMacroType.GENERAL
Function could be used in any application
|
static XyFunctionMacroType |
XyFunctionMacroType.LOAD
Function is only used to define a load
|
XyFunctionMacroType |
FunctionBuilder.TypesData.macroType
For Motion Simulation or Advanced Simulation or General Purpose
|
static XyFunctionMacroType |
XyFunctionMacroType.MATERIAL
Function is only used to define a material
|
static XyFunctionMacroType |
XyFunctionMacroType.MOTION
Function is only used in a motion application
|
static XyFunctionMacroType |
XyFunctionMacroType.RESPONSE
Function is only used to define a response
|
Modifier and Type | Method and Description |
---|---|
static XyFunctionMacroType |
XyFunctionMacroType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static XyFunctionMacroType |
XyFunctionMacroType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static XyFunctionMacroType[] |
XyFunctionMacroType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
String |
AfuManager.createRecord(XyFunctionMacroType macroType,
XyFunctionGeneralType dataType,
AfuData afuData)
Create a new AFU Data Record.
|
String |
AfuManager.editRecord(XyFunctionMacroType macroType,
XyFunctionGeneralType dataType,
int afuRecordIndex,
AfuData afuData)
Edit an existing AFU Data Record.
|
void |
FunctionBuilder.setTypes(Function.Type functionType,
XyFunctionMacroType macroType,
XyFunctionGeneralType generalType)
Sets types of a function
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.