Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
SimResultReference |
SimSolution.getResultReferenceByIndex(int resultIndex)
Returns the Result Reference at the index passed
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Modifier and Type | Method and Description |
---|---|
void |
SolutionResult.combineLoadcases(SimPart part,
SimResultReference tResultRef,
SimSolutionStep[] lcaseas,
double[] factors,
String desc)
Combine the load cases
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
ResultMeasureResultOptions |
ResultMeasureCollection.createNewResultOptions(SimSolution tSol,
SimResultReference tResultReference,
Loadcase tResultLoadcase,
Iteration tResultIteration,
boolean bAllSubiterations,
Iteration tResultSubIteration,
Result.Type pType,
Result.Component eComp)
Create a result options for result measure
License requirements: nx_masterfem ("Finite Element Modeling") . |
SolutionResult |
ResultManager.createReferenceResult(SimResultReference solution)
Creates a reference result object given a
SimResultReference
It is user's responsibility to destroy the result object once done
using ResultManager.deleteResult(nxopen.cae.Result) , in order to free up system resources. |
ResultMeasureResultOptions |
ResultMeasureCollection.createResultOptionsNew(SimSolution tSol,
SimResultReference tResultReference,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
|
void |
ResultsManipulationBuilder.setCompanionResultReference(SimResultReference tResultRef)
The companion Result Reference if action is
ResultsManipulationBuilder.Action.CREATE_COMPANION_RESULT
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX10.0.0 |
void |
AlternateFemRepresentationSourceBuilder.setResultReference(SimResultReference pResultRef)
Sets the result reference
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.