public interface AlternateFemRepresentationSourceBuilder extends Builder
AlternateFemRepresentationSourceBuilder
which can be used to create FemDataSets.
Modifier and Type | Method and Description |
---|---|
AlternateFemRepresentationSource |
commitAlternateFemRepresentationSource()
Commits the changes that have been applied to the builder and returns
the edited or newly created
AlternateFemRepresentationSource
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX12.0.0 |
void |
setFilePath(String filepath)
Sets the file path
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setLengthUnit(Unit lengthUnit)
Sets the length unit
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setMassUnit(Unit massUnit)
Sets the mass unit
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setMeshCreationMode(AlternateFemRepresentationSource.CreateMeshMode creationMode)
Sets the mesh creation mode
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setName(String name)
Sets the name of the FemDataSet
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setResultReference(SimResultReference pResultRef)
Sets the result reference
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
AlternateFemRepresentationSource commitAlternateFemRepresentationSource() throws NXException, RemoteException
AlternateFemRepresentationSource
NXException
RemoteException
void setName(String name) throws NXException, RemoteException
name
- NXException
RemoteException
void setFilePath(String filepath) throws NXException, RemoteException
filepath
- Name of the file associated to the Fem Data Set.NXException
RemoteException
void setResultReference(SimResultReference pResultRef) throws NXException, RemoteException
pResultRef
- Result Reference associated to the Fem Data Set.NXException
RemoteException
void setLengthUnit(Unit lengthUnit) throws NXException, RemoteException
lengthUnit
- Length unit used to read the data file.NXException
RemoteException
void setMassUnit(Unit massUnit) throws NXException, RemoteException
massUnit
- Mass unit used to read the data file.NXException
RemoteException
void setMeshCreationMode(AlternateFemRepresentationSource.CreateMeshMode creationMode) throws NXException, RemoteException
creationMode
- Mesh creation mode used to read the data file.NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.