Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AttributeSelectionRecipe
Represents a Selection Recipe based on attributes.
|
interface |
BoundingVolumeSelectionRecipe
Represents Bounding Volume based Selection Recipe
To obtain an instance of this object use one of the creator in SelectionRecipeCollection . |
interface |
CoordinateSelectionRecipe
Represents a single node selection recipe based on coordinates
To obtain an instance of this object use one of the creators in SelectionRecipeCollection . |
interface |
LabelRangeSelectionRecipe
Represents a Selection Recipe based on label ranges.
|
interface |
PointSelectionRecipe
Represents a single node selection recipe based on coordinates of a point
To obtain an instance of this object use one of the creators in SelectionRecipeCollection . |
interface |
SingleLabelSelectionRecipe
Represents a Selection Recipe based on a single Node Label
To obtain an instance of this object use one of the creators in SelectionRecipeCollection . |
Modifier and Type | Method and Description |
---|---|
SelectionRecipe |
SelectionRecipeCollection.copy(SelectionRecipe recipeToCopy,
String name)
Copies a Selection Recipe with all attributes and add it to the collection.
|
SelectionRecipe |
SelectionRecipeCollection.findObject(String journalIdentifier)
Finds the
SelectionRecipe with the given identifier as recorded in a journal. |
Modifier and Type | Method and Description |
---|---|
SelectionRecipe |
SelectionRecipeCollection.copy(SelectionRecipe recipeToCopy,
String name)
Copies a Selection Recipe with all attributes and add it to the collection.
|
void |
SelectionRecipeCollection.delete(SelectionRecipe[] recipes)
Delete a list of selection recipes
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
ImportSimulationBuilder.setSelectionRecipes(SelectionRecipe[] selectionRecipes)
Set Selection Recipes to import
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Modifier and Type | Method and Description |
---|---|
SelectionRecipe[] |
Composer.getGroupFromAlias(String axisAlias)
GetGroupFromAlias
License requirements: nx_masterfem ("Finite Element Modeling") . |
SelectionRecipe |
SelectionRecipeLocation.selectionRecipe()
Returns the Selection Recipe used for creating the location.
|
Modifier and Type | Method and Description |
---|---|
SelectionRecipeLocation |
ILocationsMultiPointContainer.addLocationSelectionRecipe(int indexOfDefinition,
SelectionRecipe selectionRecipe)
Adds a Selection Recipe to connection location list
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SelectionRecipeLocation.setSelectionRecipe(SelectionRecipe selectionRecipe)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.