Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.Marker |
Post.Marker.MAXIMUM_ONLY |
static Post.Marker |
Post.Marker.MINIMUM_AND_MAXIMUM |
static Post.Marker |
Post.Marker.MINIMUM_ONLY |
Modifier and Type | Method and Description |
---|---|
static Post.Marker |
Post.Marker.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Marker |
Post.Marker.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Marker[] |
Post.Marker.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewSetMarker(int postviewId,
boolean showMarker,
Post.Marker marker)
Deprecated.
Deprecated in NX9.0.0. Set
PostAnnotation show hide instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.