public static class Post.Marker extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAXIMUM_ONLY |
static int |
_MINIMUM_AND_MAXIMUM |
static int |
_MINIMUM_ONLY |
static Post.Marker |
MAXIMUM_ONLY |
static Post.Marker |
MINIMUM_AND_MAXIMUM |
static Post.Marker |
MINIMUM_ONLY |
Modifier and Type | Method and Description |
---|---|
static Post.Marker |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Marker |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Marker[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.Marker MINIMUM_AND_MAXIMUM
public static final Post.Marker MINIMUM_ONLY
public static final Post.Marker MAXIMUM_ONLY
public static final int _MINIMUM_AND_MAXIMUM
public static final int _MINIMUM_ONLY
public static final int _MAXIMUM_ONLY
public static Post.Marker valueOf(int value)
public static Post.Marker valueOf(String name)
public static Post.Marker[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.