Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CaeRegion
Represents a cae region object.
|
interface |
Laminate
|
interface |
ModelingObjectPropertyTable
Represents a Modeling Object Property Table.
|
interface |
NamedPropTableWithTargetSet
Represents a Solver Specific Modeling Object with associated target set(s)
.
|
interface |
PhysicalPropertyTable
Represents a Physical Property Table.
|
interface |
SimConstraintSet
Represents a cae constraint set object
To create a new instance of this class, use SimConstraintSetCollection.createConstraintSet(java.lang.String, java.lang.String, int) Created in NX11.0.0 |
interface |
SimLoadSet
Represents a cae load set object
To create a new instance of this class, use SimLoadSetCollection.createLoadSet(java.lang.String, java.lang.String, int) Created in NX10.0.0 |
Modifier and Type | Method and Description |
---|---|
NamedPropertyTable[] |
PropertyTable.getNamedPropertyTableArrayPropertyValue(String propertyName)
Returns the referenced array object value of the property
License requirements: None. |
NamedPropertyTable |
PropertyTable.getNamedPropertyTablePropertyValue(String propertyName)
Returns the referenced referenced named property table object value of the property
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PropertyTable.addElementsToNamedPropertyTableArrayPropertyValue(String propertyName,
NamedPropertyTable[] propertyValue)
Add elements to the referenced object array value of the property
License requirements: None. |
void |
PropertyTable.removeElementsFromNamedPropertyTableArrayPropertyValue(String propertyName,
NamedPropertyTable[] propertyValue)
Remove elements from the referenced object array value of the property
License requirements: None. |
void |
PropertyTable.setNamedPropertyTableArrayPropertyValue(String propertyName,
NamedPropertyTable[] propertyValue)
Sets the referenced object array value of the property
License requirements: None. |
void |
PropertyTable.setNamedPropertyTablePropertyValue(String propertyName,
NamedPropertyTable namedPropertyTable)
Sets the referenced named property table object value of the property
License requirements: None. |
Modifier and Type | Interface and Description |
---|---|
interface |
Element
This is the class to access a connection element
To obtain an instance of this object use the Create creator in ElementCollection . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.