Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType |
LaminateDrapingDataBuilder.ProjectionDrapingDirectionType.CSYS
Define draping direction using a coordinate system
|
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType |
LaminateDrapingDataBuilder.ProjectionDrapingDirectionType.MOV
Define draping direction using MOVs
|
Modifier and Type | Method and Description |
---|---|
LaminateDrapingDataBuilder.ProjectionDrapingDirectionType |
LaminateDrapingDataBuilder.projectionDirectionOption()
Returns the projection draping direction option
License requirements: None. |
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType |
LaminateDrapingDataBuilder.ProjectionDrapingDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType |
LaminateDrapingDataBuilder.ProjectionDrapingDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType[] |
LaminateDrapingDataBuilder.ProjectionDrapingDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LaminateDrapingDataBuilder.setProjectionDirectionOption(LaminateDrapingDataBuilder.ProjectionDrapingDirectionType projectionDirectionOption)
License requirements: nx_lam_comp_adv ("Laminate Composites Advanced") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.