public static class LaminateDrapingDataBuilder.ProjectionDrapingDirectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CSYS
Define draping direction using a coordinate system
|
static int |
_MOV
Define draping direction using MOVs
|
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType |
CSYS
Define draping direction using a coordinate system
|
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType |
MOV
Define draping direction using MOVs
|
Modifier and Type | Method and Description |
---|---|
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LaminateDrapingDataBuilder.ProjectionDrapingDirectionType MOV
public static final LaminateDrapingDataBuilder.ProjectionDrapingDirectionType CSYS
public static final int _MOV
public static final int _CSYS
public static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType valueOf(int value)
public static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType valueOf(String name)
public static LaminateDrapingDataBuilder.ProjectionDrapingDirectionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.