Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AssyFEModel
This class represents an Assembly Finite Element Model.
|
interface |
AtvSet
This is the class representing a Atv result set.
|
interface |
DataProcessing
Represents a
DataProcessing . |
interface |
DataProcessingBlock
Represents a
DataProcessingBlock . |
interface |
FEModelOccurrence
This class represents a Finite Element Model Occurrence.
|
interface |
FrfSet
This is the class representing a FRF set.
|
interface |
ModeSet
This is the class representing a Mode set.
|
interface |
SimLoadRecipe
This is the class handling the attributes of a load recipe.
|
interface |
SimResultReference
Represents a Result Reference in the .sim files.
|
interface |
SimSimulationObject
Represents a simulation object.
|
Modifier and Type | Method and Description |
---|---|
IPostScenarioDataSource |
PostScenarioParameters.dataSource()
Deprecated.
Deprecated in NX12.0.0. Data Sources are now added through
PostScenarioManager.dataSources() . Alternatively, PostScenarioParameters.setPreferredDataSources(nxopen.cae.DataSource[]) can be used to configure the default configuration of a scenario. Setting this attribute has the same effect as SetPreferredDataSources(value).
|
IPostScenarioDataSource |
DataSourceBuilder.sourceObject()
Returns the selected source object
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Modifier and Type | Method and Description |
---|---|
void |
PostScenarioParameters.setDataSource(IPostScenarioDataSource dataSource)
Deprecated.
Deprecated in NX12.0.0. Data Sources are now added through
PostScenarioManager.dataSources() . Alternatively, PostScenarioParameters.setPreferredDataSources(nxopen.cae.DataSource[]) can be used to configure the default configuration of a scenario. Setting this attribute has the same effect as SetPreferredDataSources(value).
|
void |
DataSourceBuilder.setSourceObject(IPostScenarioDataSource sourceObject)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.