Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CartesianCoordinateSystem
Represents a cartesian coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCoordinateSystem(nxopen.Point3d, nxopen.Matrix3x3, boolean) Created in NX4.0.0 |
interface |
CoordinateSystem
Represents a coordinate system
This is an abstract class . |
interface |
CylindricalCoordinateSystem
Represents a cylindrical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCylindricalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
interface |
PhysicalMaterial
Represents Physical Material .
|
interface |
SphericalCoordinateSystem
Represents a spherical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createSphericalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
CaeGroup
Represents a group class
CaeGroup . |
interface |
CaeRegion
Represents a cae region object.
|
interface |
DependentMesh
Represents Mesh Recipe
To create or edit an instance of this class, use DependentMeshBuilder Created in NX5.0.0 |
interface |
FEElement
Represents a Finite Element.
|
interface |
FENode
Represents a Finite Element Node.
|
interface |
HybridMesh
Represents swept Mesh
To create or edit an instance of this class, use Mesh3dHybridBuilder Created in NX11.0.0 |
interface |
Laminate
|
interface |
MappedMesh
Represents Mesh Recipe
To create or edit an instance of this class, use MappedMeshBuilder Created in NX5.0.0 |
interface |
Mesh
Represents a Mesh.
|
interface |
Mesh0d
Represents 0d Mesh
To create or edit an instance of this class, use Mesh0dBuilder Created in NX6.0.0 |
interface |
Mesh1d
Represents 1d Mesh
To create or edit an instance of this class, use Mesh1dBuilder Created in NX6.0.0 |
interface |
Mesh2d
Represents 2d Mesh
This is an abstract class . |
interface |
Mesh2dFree
Represents 2d Mesh
To create or edit an instance of this class, use Mesh2dBuilder Created in NX6.0.0 |
interface |
Mesh3d
Represents 3d Mesh
To create or edit an instance of this class, use Mesh3dTetBuilder Created in NX6.0.0 |
interface |
MeshFollower
Represents Mesh Recipe
This is an abstract class . |
interface |
MeshShellFromSolid
Represents 2d Mesh that follows 3d mesh
To create or edit an instance of this class, use SurfaceCoatBuilder Created in NX7.5.0 |
interface |
ModelingObjectPropertyTable
Represents a Modeling Object Property Table.
|
interface |
PhysicalPropertyTable
Represents a Physical Property Table.
|
interface |
PrimitiveMesh
Represents Primitive Mesh
To create or edit an instance of this class, use PrimitiveMeshBuilder Created in NX7.5.0 |
interface |
PrimitiveRecipeMesh
Represents a primitive recipe mesh.
|
interface |
RecipeConvexMesh
Represents a convex mesh.
|
interface |
RecipeOpenDuctMesh
Represents a open duct mesh.
|
interface |
RecipeSurfaceWrap
Represents 2d mesh associated to fluid domain body, all from surface wrapper.
|
interface |
ShipMeshAutomation
Represents Ship Mesh Automation
This is an abstract class . |
interface |
SimBC
Represents BC class which is a superclass to
SimLoad and SimConstraint . |
interface |
SimConstraint
Represents a constraint
To create a new instance of this class, use SimConstraintCollection.createConstraint(java.lang.String, java.lang.String) Created in NX4.0.0 |
interface |
SimLoad
Represents a load
To create a new instance of this class, use SimLoadCollection.createLoad(java.lang.String, java.lang.String) Created in NX4.0.0 |
interface |
SimLoadSet
Represents a cae load set object
To create a new instance of this class, use SimLoadSetCollection.createLoadSet(java.lang.String, java.lang.String, int) Created in NX10.0.0 |
interface |
SimSimulationObject
Represents a simulation object.
|
interface |
SweptMesh
Represents swept Mesh
To create or edit an instance of this class, use Mesh3dHexBuilder Created in NX6.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
Element
This is the class to access a connection element
To obtain an instance of this object use the Create creator in ElementCollection . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.