Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FreeBodyResultsBuilder.OutputUnits |
FreeBodyResultsBuilder.OutputUnits.DEFAULT
same as Solver Deck Unit
|
static FreeBodyResultsBuilder.OutputUnits |
FreeBodyResultsBuilder.OutputUnits.FT_POUND_FORCE
Load unit = "lbf", Moment unit lbf-ft
|
static FreeBodyResultsBuilder.OutputUnits |
FreeBodyResultsBuilder.OutputUnits.IN_POUND_FORCE
Load unit = "lbf", Moment unit lbf-in
|
static FreeBodyResultsBuilder.OutputUnits |
FreeBodyResultsBuilder.OutputUnits.METER_NEWTON
Load unit = "N", Moment unit N-m
|
static FreeBodyResultsBuilder.OutputUnits |
FreeBodyResultsBuilder.OutputUnits.MILLI_MILLINEWTON
Load unit = "mN", Moment unit N-mm
|
static FreeBodyResultsBuilder.OutputUnits |
FreeBodyResultsBuilder.OutputUnits.MILLI_NEWTON
Load unit = "N", Moment unit N-mm
|
Modifier and Type | Method and Description |
---|---|
FreeBodyResultsBuilder.OutputUnits |
FreeBodyResultsBuilder.getOutputUnits()
Output Units
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
static FreeBodyResultsBuilder.OutputUnits |
FreeBodyResultsBuilder.OutputUnits.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FreeBodyResultsBuilder.OutputUnits |
FreeBodyResultsBuilder.OutputUnits.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FreeBodyResultsBuilder.OutputUnits[] |
FreeBodyResultsBuilder.OutputUnits.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FreeBodyResultsBuilder.setOutputUnits(FreeBodyResultsBuilder.OutputUnits units)
Output Units
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.