public static class FreeBodyResultsBuilder.OutputUnits extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEFAULT
same as Solver Deck Unit
|
static int |
_FT_POUND_FORCE
Load unit = "lbf", Moment unit lbf-ft
|
static int |
_IN_POUND_FORCE
Load unit = "lbf", Moment unit lbf-in
|
static int |
_METER_NEWTON
Load unit = "N", Moment unit N-m
|
static int |
_MILLI_MILLINEWTON
Load unit = "mN", Moment unit N-mm
|
static int |
_MILLI_NEWTON
Load unit = "N", Moment unit N-mm
|
static FreeBodyResultsBuilder.OutputUnits |
DEFAULT
same as Solver Deck Unit
|
static FreeBodyResultsBuilder.OutputUnits |
FT_POUND_FORCE
Load unit = "lbf", Moment unit lbf-ft
|
static FreeBodyResultsBuilder.OutputUnits |
IN_POUND_FORCE
Load unit = "lbf", Moment unit lbf-in
|
static FreeBodyResultsBuilder.OutputUnits |
METER_NEWTON
Load unit = "N", Moment unit N-m
|
static FreeBodyResultsBuilder.OutputUnits |
MILLI_MILLINEWTON
Load unit = "mN", Moment unit N-mm
|
static FreeBodyResultsBuilder.OutputUnits |
MILLI_NEWTON
Load unit = "N", Moment unit N-mm
|
Modifier and Type | Method and Description |
---|---|
static FreeBodyResultsBuilder.OutputUnits |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FreeBodyResultsBuilder.OutputUnits |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FreeBodyResultsBuilder.OutputUnits[] |
values()
Returns an array that contains the values for this enum.
|
public static final FreeBodyResultsBuilder.OutputUnits DEFAULT
public static final FreeBodyResultsBuilder.OutputUnits MILLI_NEWTON
public static final FreeBodyResultsBuilder.OutputUnits MILLI_MILLINEWTON
public static final FreeBodyResultsBuilder.OutputUnits METER_NEWTON
public static final FreeBodyResultsBuilder.OutputUnits FT_POUND_FORCE
public static final FreeBodyResultsBuilder.OutputUnits IN_POUND_FORCE
public static final int _DEFAULT
public static final int _MILLI_NEWTON
public static final int _MILLI_MILLINEWTON
public static final int _METER_NEWTON
public static final int _FT_POUND_FORCE
public static final int _IN_POUND_FORCE
public static FreeBodyResultsBuilder.OutputUnits valueOf(int value)
public static FreeBodyResultsBuilder.OutputUnits valueOf(String name)
public static FreeBodyResultsBuilder.OutputUnits[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.