Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static FluidDomainBuilder.OutputOptionsType |
FluidDomainBuilder.OutputOptionsType.BODY_ONLY
The output type specified as only body generation.
|
static FluidDomainBuilder.OutputOptionsType |
FluidDomainBuilder.OutputOptionsType.BODYAND_MESH
The output type specified as body and mesh generation.
|
static FluidDomainBuilder.OutputOptionsType |
FluidDomainBuilder.OutputOptionsType.MESH_ONLY
The output type specified as only mesh genberation.
|
Modifier and Type | Method and Description |
---|---|
FluidDomainBuilder.OutputOptionsType |
FluidDomainBuilder.outputType()
Returns the output selection type represented by
FluidDomainBuilder.OutputOptionsType
License requirements: None. |
static FluidDomainBuilder.OutputOptionsType |
FluidDomainBuilder.OutputOptionsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FluidDomainBuilder.OutputOptionsType |
FluidDomainBuilder.OutputOptionsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FluidDomainBuilder.OutputOptionsType[] |
FluidDomainBuilder.OutputOptionsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FluidDomainBuilder.setOutputType(FluidDomainBuilder.OutputOptionsType type)
License requirements: nx_adv_fluid_mod ("NX Advanced Fluid Modeling - Basic") OR sc_acou_meshing (" SC Acoustic Meshing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.