public static class FluidDomainBuilder.OutputOptionsType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BODY_ONLY
The output type specified as only body generation.
|
static int |
_BODYAND_MESH
The output type specified as body and mesh generation.
|
static int |
_MESH_ONLY
The output type specified as only mesh genberation.
|
static FluidDomainBuilder.OutputOptionsType |
BODY_ONLY
The output type specified as only body generation.
|
static FluidDomainBuilder.OutputOptionsType |
BODYAND_MESH
The output type specified as body and mesh generation.
|
static FluidDomainBuilder.OutputOptionsType |
MESH_ONLY
The output type specified as only mesh genberation.
|
Modifier and Type | Method and Description |
---|---|
static FluidDomainBuilder.OutputOptionsType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FluidDomainBuilder.OutputOptionsType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FluidDomainBuilder.OutputOptionsType[] |
values()
Returns an array that contains the values for this enum.
|
public static final FluidDomainBuilder.OutputOptionsType BODY_ONLY
public static final FluidDomainBuilder.OutputOptionsType BODYAND_MESH
public static final FluidDomainBuilder.OutputOptionsType MESH_ONLY
public static final int _BODY_ONLY
public static final int _BODYAND_MESH
public static final int _MESH_ONLY
public static FluidDomainBuilder.OutputOptionsType valueOf(int value)
public static FluidDomainBuilder.OutputOptionsType valueOf(String name)
public static FluidDomainBuilder.OutputOptionsType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.