Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementRotateBuilder.CopyType |
ElementRotateBuilder.CopyType.COPY_ROTATE
first copy elements then rotate the copies
|
static ElementRotateBuilder.CopyType |
ElementRotateBuilder.CopyType.ROTATE_ONLY
rotate without copying elements
|
Modifier and Type | Method and Description |
---|---|
ElementRotateBuilder.CopyType |
ElementRotateBuilder.copyOption()
Returns the copy option .
|
static ElementRotateBuilder.CopyType |
ElementRotateBuilder.CopyType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementRotateBuilder.CopyType |
ElementRotateBuilder.CopyType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementRotateBuilder.CopyType[] |
ElementRotateBuilder.CopyType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementRotateBuilder.setCopyOption(ElementRotateBuilder.CopyType inCopyoption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.