public static class ElementRotateBuilder.CopyType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COPY_ROTATE
first copy elements then rotate the copies
|
static int |
_ROTATE_ONLY
rotate without copying elements
|
static ElementRotateBuilder.CopyType |
COPY_ROTATE
first copy elements then rotate the copies
|
static ElementRotateBuilder.CopyType |
ROTATE_ONLY
rotate without copying elements
|
Modifier and Type | Method and Description |
---|---|
static ElementRotateBuilder.CopyType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementRotateBuilder.CopyType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementRotateBuilder.CopyType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ElementRotateBuilder.CopyType ROTATE_ONLY
public static final ElementRotateBuilder.CopyType COPY_ROTATE
public static final int _ROTATE_ONLY
public static final int _COPY_ROTATE
public static ElementRotateBuilder.CopyType valueOf(int value)
public static ElementRotateBuilder.CopyType valueOf(String name)
public static ElementRotateBuilder.CopyType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.