Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static DurSpecialistSuperpositionEventBuilder.RangeType |
DurSpecialistSuperpositionEventBuilder.RangeType.FULL_HISTORY
All the points of the load history are taken
|
static DurSpecialistSuperpositionEventBuilder.RangeType |
DurSpecialistSuperpositionEventBuilder.RangeType.SUB_RANGE
The load history is restricted to a range
|
Modifier and Type | Method and Description |
---|---|
DurSpecialistSuperpositionEventBuilder.RangeType |
DurSpecialistSuperpositionEventBuilder.range()
Returns the interval range.
|
static DurSpecialistSuperpositionEventBuilder.RangeType |
DurSpecialistSuperpositionEventBuilder.RangeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurSpecialistSuperpositionEventBuilder.RangeType |
DurSpecialistSuperpositionEventBuilder.RangeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurSpecialistSuperpositionEventBuilder.RangeType[] |
DurSpecialistSuperpositionEventBuilder.RangeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DurSpecialistSuperpositionEventBuilder.setRange(DurSpecialistSuperpositionEventBuilder.RangeType type)
License requirements: nx_adv_durability ("NX Advanced Durability") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.