public static class DurSpecialistSuperpositionEventBuilder.RangeType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FULL_HISTORY
All the points of the load history are taken
|
static int |
_SUB_RANGE
The load history is restricted to a range
|
static DurSpecialistSuperpositionEventBuilder.RangeType |
FULL_HISTORY
All the points of the load history are taken
|
static DurSpecialistSuperpositionEventBuilder.RangeType |
SUB_RANGE
The load history is restricted to a range
|
Modifier and Type | Method and Description |
---|---|
static DurSpecialistSuperpositionEventBuilder.RangeType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurSpecialistSuperpositionEventBuilder.RangeType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurSpecialistSuperpositionEventBuilder.RangeType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DurSpecialistSuperpositionEventBuilder.RangeType FULL_HISTORY
public static final DurSpecialistSuperpositionEventBuilder.RangeType SUB_RANGE
public static final int _FULL_HISTORY
public static final int _SUB_RANGE
public static DurSpecialistSuperpositionEventBuilder.RangeType valueOf(int value)
public static DurSpecialistSuperpositionEventBuilder.RangeType valueOf(String name)
public static DurSpecialistSuperpositionEventBuilder.RangeType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.