Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static DurSpecialistSuperpositionEventBuilder.MatchingType |
DurSpecialistSuperpositionEventBuilder.MatchingType.AUTOMATIC
The connections are done automatically
|
static DurSpecialistSuperpositionEventBuilder.MatchingType |
DurSpecialistSuperpositionEventBuilder.MatchingType.MANUAL
The connections are done manually
|
Modifier and Type | Method and Description |
---|---|
DurSpecialistSuperpositionEventBuilder.MatchingType |
DurSpecialistSuperpositionEventBuilder.matching()
Returns the matching.
|
static DurSpecialistSuperpositionEventBuilder.MatchingType |
DurSpecialistSuperpositionEventBuilder.MatchingType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurSpecialistSuperpositionEventBuilder.MatchingType |
DurSpecialistSuperpositionEventBuilder.MatchingType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurSpecialistSuperpositionEventBuilder.MatchingType[] |
DurSpecialistSuperpositionEventBuilder.MatchingType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DurSpecialistSuperpositionEventBuilder.setMatching(DurSpecialistSuperpositionEventBuilder.MatchingType type)
License requirements: nx_adv_durability ("NX Advanced Durability") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.