public static class DurSpecialistSuperpositionEventBuilder.MatchingType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
The connections are done automatically
|
static int |
_MANUAL
The connections are done manually
|
static DurSpecialistSuperpositionEventBuilder.MatchingType |
AUTOMATIC
The connections are done automatically
|
static DurSpecialistSuperpositionEventBuilder.MatchingType |
MANUAL
The connections are done manually
|
Modifier and Type | Method and Description |
---|---|
static DurSpecialistSuperpositionEventBuilder.MatchingType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurSpecialistSuperpositionEventBuilder.MatchingType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurSpecialistSuperpositionEventBuilder.MatchingType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DurSpecialistSuperpositionEventBuilder.MatchingType AUTOMATIC
public static final DurSpecialistSuperpositionEventBuilder.MatchingType MANUAL
public static final int _AUTOMATIC
public static final int _MANUAL
public static DurSpecialistSuperpositionEventBuilder.MatchingType valueOf(int value)
public static DurSpecialistSuperpositionEventBuilder.MatchingType valueOf(String name)
public static DurSpecialistSuperpositionEventBuilder.MatchingType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.