Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static DurSpecialistBlockLoadEventBuilder.PatternType |
DurSpecialistBlockLoadEventBuilder.PatternType.ALTERNATING
between value and -value
|
static DurSpecialistBlockLoadEventBuilder.PatternType |
DurSpecialistBlockLoadEventBuilder.PatternType.FREE
between two values
|
static DurSpecialistBlockLoadEventBuilder.PatternType |
DurSpecialistBlockLoadEventBuilder.PatternType.SWELLING
between 0 and value
|
Modifier and Type | Method and Description |
---|---|
DurSpecialistBlockLoadEventBuilder.PatternType |
DurSpecialistBlockLoadEventBuilder.pattern()
Returns the pattern.
|
static DurSpecialistBlockLoadEventBuilder.PatternType |
DurSpecialistBlockLoadEventBuilder.PatternType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurSpecialistBlockLoadEventBuilder.PatternType |
DurSpecialistBlockLoadEventBuilder.PatternType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurSpecialistBlockLoadEventBuilder.PatternType[] |
DurSpecialistBlockLoadEventBuilder.PatternType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DurSpecialistBlockLoadEventBuilder.setPattern(DurSpecialistBlockLoadEventBuilder.PatternType type)
License requirements: nx_adv_durability ("NX Advanced Durability") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.