public static class DurSpecialistBlockLoadEventBuilder.PatternType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALTERNATING
between value and -value
|
static int |
_FREE
between two values
|
static int |
_SWELLING
between 0 and value
|
static DurSpecialistBlockLoadEventBuilder.PatternType |
ALTERNATING
between value and -value
|
static DurSpecialistBlockLoadEventBuilder.PatternType |
FREE
between two values
|
static DurSpecialistBlockLoadEventBuilder.PatternType |
SWELLING
between 0 and value
|
Modifier and Type | Method and Description |
---|---|
static DurSpecialistBlockLoadEventBuilder.PatternType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DurSpecialistBlockLoadEventBuilder.PatternType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DurSpecialistBlockLoadEventBuilder.PatternType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DurSpecialistBlockLoadEventBuilder.PatternType SWELLING
public static final DurSpecialistBlockLoadEventBuilder.PatternType ALTERNATING
public static final DurSpecialistBlockLoadEventBuilder.PatternType FREE
public static final int _SWELLING
public static final int _ALTERNATING
public static final int _FREE
public static DurSpecialistBlockLoadEventBuilder.PatternType valueOf(int value)
public static DurSpecialistBlockLoadEventBuilder.PatternType valueOf(String name)
public static DurSpecialistBlockLoadEventBuilder.PatternType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.