Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CreateJtBuilder.Component |
CreateJtBuilder.Component.CURRENT
Value represents component used to create result parameter
|
static CreateJtBuilder.Component |
CreateJtBuilder.Component.PRIMARY
Value represents all primary components
|
static CreateJtBuilder.Component |
CreateJtBuilder.Component.UNKNOWN
Value has an Unknown type
|
Modifier and Type | Method and Description |
---|---|
static CreateJtBuilder.Component |
CreateJtBuilder.Component.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CreateJtBuilder.Component |
CreateJtBuilder.Component.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CreateJtBuilder.Component[] |
CreateJtBuilder.Component.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CreateJtBuilder.setExportData(ResultParameters[] parameters,
int[] templateIds,
CreateJtBuilder.Component[] componentToExport)
The result parameters
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.