public interface CreateJtBuilder extends Builder
CreateJtBuilder
Session.resultManager()
. Modifier and Type | Interface and Description |
---|---|
static class |
CreateJtBuilder.Component
This option is used to set the component for export
|
Modifier and Type | Method and Description |
---|---|
void |
setExportData(ResultParameters[] parameters,
int[] templateIds,
CreateJtBuilder.Component[] componentToExport)
The result parameters
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
void |
setOutputFile(String outputFile)
The output file
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
void |
setResult(Result result)
The result
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
void setResult(Result result) throws NXException, RemoteException
result
- set resultNXException
RemoteException
void setExportData(ResultParameters[] parameters, int[] templateIds, CreateJtBuilder.Component[] componentToExport) throws NXException, RemoteException
parameters
- set result parameterstemplateIds
- set template Id per result parametercomponentToExport
- set template Id per result parameterNXException
RemoteException
void setOutputFile(String outputFile) throws NXException, RemoteException
outputFile
- set output fileNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.