Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CaePart.FieldApplicationType |
CaePart.FieldApplicationType.SIGNAL_PROCESSING
Application which allows to specify additional attributes (e.g. acoustical weighting) on a field
|
Modifier and Type | Method and Description |
---|---|
static CaePart.FieldApplicationType |
CaePart.FieldApplicationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaePart.FieldApplicationType |
CaePart.FieldApplicationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaePart.FieldApplicationType[] |
CaePart.FieldApplicationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
IApplication |
CaePart.getApplication(CaePart.FieldApplicationType applicationType)
Get the application which corresponds to the specified type.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.