public static class CaePart.FieldApplicationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SIGNAL_PROCESSING
Application which allows to specify additional attributes (e.g. acoustical weighting) on a field
|
static CaePart.FieldApplicationType |
SIGNAL_PROCESSING
Application which allows to specify additional attributes (e.g. acoustical weighting) on a field
|
Modifier and Type | Method and Description |
---|---|
static CaePart.FieldApplicationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaePart.FieldApplicationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaePart.FieldApplicationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final CaePart.FieldApplicationType SIGNAL_PROCESSING
public static final int _SIGNAL_PROCESSING
public static CaePart.FieldApplicationType valueOf(int value)
public static CaePart.FieldApplicationType valueOf(String name)
public static CaePart.FieldApplicationType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.