Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CaeElementAssociatedDataUtilsVectorChoiceType |
CaeElementAssociatedDataUtilsVectorChoiceType.HORIZONTAL
The vector is defined to be horizontal.
|
CaeElementAssociatedDataUtilsVectorChoiceType |
ElementAssociatedDataUtils.AskBeamData.vectortype
Orientation vector type.
|
static CaeElementAssociatedDataUtilsVectorChoiceType |
CaeElementAssociatedDataUtilsVectorChoiceType.VERTICAL
The vector is defined to be vertical.
|
Modifier and Type | Method and Description |
---|---|
static CaeElementAssociatedDataUtilsVectorChoiceType |
CaeElementAssociatedDataUtilsVectorChoiceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaeElementAssociatedDataUtilsVectorChoiceType |
CaeElementAssociatedDataUtilsVectorChoiceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaeElementAssociatedDataUtilsVectorChoiceType[] |
CaeElementAssociatedDataUtilsVectorChoiceType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.