public class CaeElementAssociatedDataUtilsVectorChoiceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL
The vector is defined to be horizontal.
|
static int |
_VERTICAL
The vector is defined to be vertical.
|
static CaeElementAssociatedDataUtilsVectorChoiceType |
HORIZONTAL
The vector is defined to be horizontal.
|
static CaeElementAssociatedDataUtilsVectorChoiceType |
VERTICAL
The vector is defined to be vertical.
|
Modifier and Type | Method and Description |
---|---|
static CaeElementAssociatedDataUtilsVectorChoiceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaeElementAssociatedDataUtilsVectorChoiceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaeElementAssociatedDataUtilsVectorChoiceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final CaeElementAssociatedDataUtilsVectorChoiceType HORIZONTAL
public static final CaeElementAssociatedDataUtilsVectorChoiceType VERTICAL
public static final int _HORIZONTAL
public static final int _VERTICAL
public static CaeElementAssociatedDataUtilsVectorChoiceType valueOf(int value)
public static CaeElementAssociatedDataUtilsVectorChoiceType valueOf(String name)
public static CaeElementAssociatedDataUtilsVectorChoiceType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.