Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CaeBoundingVolumePrimitiveContainment |
CaeBoundingVolumePrimitiveContainment.INSIDE
completely inside the primitive
|
static CaeBoundingVolumePrimitiveContainment |
CaeBoundingVolumePrimitiveContainment.INSIDE_CROSSING
completely inside or partially inside the primitive
|
Modifier and Type | Method and Description |
---|---|
CaeBoundingVolumePrimitiveContainment |
BoundingVolumePrimitive.containment()
Returns the contaiment for the Bounding Volume Primitive.
|
static CaeBoundingVolumePrimitiveContainment |
CaeBoundingVolumePrimitiveContainment.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaeBoundingVolumePrimitiveContainment |
CaeBoundingVolumePrimitiveContainment.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaeBoundingVolumePrimitiveContainment[] |
CaeBoundingVolumePrimitiveContainment.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BoundingVolumePrimitive.setContainment(CaeBoundingVolumePrimitiveContainment containment)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.