public class CaeBoundingVolumePrimitiveContainment extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INSIDE
completely inside the primitive
|
static int |
_INSIDE_CROSSING
completely inside or partially inside the primitive
|
static CaeBoundingVolumePrimitiveContainment |
INSIDE
completely inside the primitive
|
static CaeBoundingVolumePrimitiveContainment |
INSIDE_CROSSING
completely inside or partially inside the primitive
|
Modifier and Type | Method and Description |
---|---|
static CaeBoundingVolumePrimitiveContainment |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CaeBoundingVolumePrimitiveContainment |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CaeBoundingVolumePrimitiveContainment[] |
values()
Returns an array that contains the values for this enum.
|
public static final CaeBoundingVolumePrimitiveContainment INSIDE
public static final CaeBoundingVolumePrimitiveContainment INSIDE_CROSSING
public static final int _INSIDE
public static final int _INSIDE_CROSSING
public static CaeBoundingVolumePrimitiveContainment valueOf(int value)
public static CaeBoundingVolumePrimitiveContainment valueOf(String name)
public static CaeBoundingVolumePrimitiveContainment[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.