Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CAEWeldConnectionBuilder.WeldTypeEnum |
CAEWeldConnectionBuilder.WeldTypeEnum.POINT_TO_POINT_DIRECT
It's a point to point direct weldconnection,mesh points are created during weld connection
|
static CAEWeldConnectionBuilder.WeldTypeEnum |
CAEWeldConnectionBuilder.WeldTypeEnum.POINT_TO_POINT_INDIRECT
It's a point to point in-direct weldconnection,RBE3 elements are created during weld connection
|
static CAEWeldConnectionBuilder.WeldTypeEnum |
CAEWeldConnectionBuilder.WeldTypeEnum.POINT_TO_POINT3D_WELD
It's a point to point in-direct weldconnection,3D elements are created during weld connection
|
Modifier and Type | Method and Description |
---|---|
static CAEWeldConnectionBuilder.WeldTypeEnum |
CAEWeldConnectionBuilder.WeldTypeEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAEWeldConnectionBuilder.WeldTypeEnum |
CAEWeldConnectionBuilder.WeldTypeEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAEWeldConnectionBuilder.WeldTypeEnum[] |
CAEWeldConnectionBuilder.WeldTypeEnum.values()
Returns an array that contains the values for this enum.
|
CAEWeldConnectionBuilder.WeldTypeEnum |
CAEWeldConnectionBuilder.weldType()
Returns the weld connection type
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
CAEWeldConnectionBuilder.setWeldType(CAEWeldConnectionBuilder.WeldTypeEnum weldType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.