public static class CAEWeldConnectionBuilder.WeldTypeEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_POINT_TO_POINT_DIRECT
It's a point to point direct weldconnection,mesh points are created during weld connection
|
static int |
_POINT_TO_POINT_INDIRECT
It's a point to point in-direct weldconnection,RBE3 elements are created during weld connection
|
static int |
_POINT_TO_POINT3D_WELD
It's a point to point in-direct weldconnection,3D elements are created during weld connection
|
static CAEWeldConnectionBuilder.WeldTypeEnum |
POINT_TO_POINT_DIRECT
It's a point to point direct weldconnection,mesh points are created during weld connection
|
static CAEWeldConnectionBuilder.WeldTypeEnum |
POINT_TO_POINT_INDIRECT
It's a point to point in-direct weldconnection,RBE3 elements are created during weld connection
|
static CAEWeldConnectionBuilder.WeldTypeEnum |
POINT_TO_POINT3D_WELD
It's a point to point in-direct weldconnection,3D elements are created during weld connection
|
Modifier and Type | Method and Description |
---|---|
static CAEWeldConnectionBuilder.WeldTypeEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAEWeldConnectionBuilder.WeldTypeEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAEWeldConnectionBuilder.WeldTypeEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final CAEWeldConnectionBuilder.WeldTypeEnum POINT_TO_POINT_DIRECT
public static final CAEWeldConnectionBuilder.WeldTypeEnum POINT_TO_POINT_INDIRECT
public static final CAEWeldConnectionBuilder.WeldTypeEnum POINT_TO_POINT3D_WELD
public static final int _POINT_TO_POINT_DIRECT
public static final int _POINT_TO_POINT_INDIRECT
public static final int _POINT_TO_POINT3D_WELD
public static CAEWeldConnectionBuilder.WeldTypeEnum valueOf(int value)
public static CAEWeldConnectionBuilder.WeldTypeEnum valueOf(String name)
public static CAEWeldConnectionBuilder.WeldTypeEnum[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.